Technical FAQs

Ask a Question

How do we set up Auto restart in ATS22?

Issue:
How do we set up Auto restart in ATS22?
 
Product Line:
ATS22
 
Environment:
Auto restart
 
Cause:
 n/a

Resolution:

There is no Auto restart option available in ATS22. One has to manually restart the soft starter when there is an occurrence of a fault that requires power recycle. 

 
Was this helpful?
What can we do to improve the information ?