Technical FAQs

Ask a Question

What needs to be done to the ATS48 soft starter if you want to add a motor disconnect switch to open motor?

Issue:
What needs to be done to the ATS48 soft starter if you want to add a motor disconnect switch to open motor?

Product Line:
ATS48

Environment:
All

Cause:
Need to remove the run command before opening the motor disconnect.

Resolution:
You will need to open the run command and set up normal stop type as freewheel stop or set up a logic input for freewheel stop. 
 
Was this helpful?
What can we do to improve the information ?