Technical FAQs

Ask a Question

Conext CL is not communicating using Conext Insight

Issue:
Conext Insight is not able to register and log information on the Conext CL models.
 
Environment:
Applications that use the Conext CL inverters.
 

Product Line:
Conext CL 25NA, Conext CL 18NA, Conext CL60NA

Cause:
Conext Insight support has been disconiting discontinued for all Conext CLNA Solar Inverters 

Resolution:

Customers can work with third party monitoring solutions such as Also Energy or SolarEdge as an alternative



 
Was this helpful?
What can we do to improve the information ?