Technical FAQs

Ask a Question

What is the smallest Active Front End Process drive available?

Issue:
What is the smallest Active Front End Process drive available?

Product line:
Altivar Process drives, ATV600 and ATV900 series

Environment:
Only those units with the Active Front End option installed.

Cause:
Information unavailable in current literature.

Resolution:
The lowest horsepower Active Front End process drive currently available is rated for 125 Horsepower.



 
Was this helpful?
What can we do to improve the information ?