Technical FAQs

Ask a Question

What does suffix 1614 mean on a breaker?

Issue:
What does suffix 1614 mean on a breaker?

Product Line:
Circuit Breakers

Environment:
Applies to breaker types FA, FAL, FH, FHL, FIJ, FIL, KAL, KAP, KA, KC, KHL, KHP, KH, KIJ, KIL, LAF, LAL, MAL, ME, MHF, MHL, PAF, PHF

Resolution:
Suffix 1614 is obsolete and is replaced with suffix 1595.
Suffix 1595 consists of the following:
  • 2A2A Auxiliary Contacts (suffix 1352)
  • 120Vac Undervoltage Trip (suffix 1121)

 

Was this helpful?
What can we do to improve the information ?