Technical FAQs

Ask a Question

What wire sizes do the ZBE contact blocks with spring or screw terminals accept?

Issue:
What wire sizes can be used on the 22 mm operators? 

Product Line:
22mm XB4 and XB5 Harmony Pushbuttons

Environment:
US Product

Cause:
Installation

Resolution:
The wire sizes, In mm^2, are:
Min: 1 x 0.22 without cable end
Max: 2 x 1.5 with cable end
Was this helpful?
What can we do to improve the information ?