Technical FAQs

Ask a Question

OBSOLETE - (See FA317834) What is a DP4075 Circuit Breaker?

Product Line:
QO/B and HOM
 
Cause:
Cannot find it in the Digest
 
Resolution:
DP4075 is the UL issue number for a QO/B or Homeline breaker. This does not identify the breaker. To determine what the breaker is we would need to know the number of poles, ampere rating and panel to tell what breaker can be used.
 
 
Was this helpful?
What can we do to improve the information ?