Technical FAQs

Ask a Question

Is ATV12 a direct replacement of ATV11?

Issue:
Is ATV12 a direct replacement of ATV11?

Product Line:
Altivar 12

Environment:
All

Cause:
Need to replace an ATV11

Resolution:
ATV12 is not a direct replacement of ATV11. ATV11 has 15Vdc supply while ATV12 has 24Vdc supply. All new series of drives come with 24Vdc supply. ATV12 replaces ATV11 only in regards to the functionality.  
Was this helpful?
What can we do to improve the information ?