Technical FAQs

Ask a Question

Can the LUCC reverser module be used in a single phase reversing application?

Issue:
Can the TeSys U self protected starter be used in a single phase reversing application? 

Product Line:
TeSys U Starters - GIC Product

Environment:
US Product

Cause:
Product selection - application assistance

Resolution: 
Depending on the motor in use, reversing the rotation of a single phase motor requires either to wire differently the rotor or the stator winding(s), or to change the wire the starting capacitor is connected to, etc....
In any of these cases, the modification is to be done at the motor itself.
So, no possibility to change the direction of rotation with TeSys U and LUCC, whatever the TeSys U reversing solution used, LU2B or LU6M.
LUCC is not compatible with LU2B nor with LU6M.
Was this helpful?
What can we do to improve the information ?