Technical FAQs

Ask a Question

INTERNAL: How to find trip curves in the Download center

Issue:
The trip curves in the Download center are not found in the same manner as they were in the Classic Technical Library.

Product Line:
Circuit Breakers

Environment:
Applies to trip curves on the Schneider US site

Resolution:
To locate circuit breaker trip curves in the Download Center, follow these steps:
  1. Go to the Download Center  https://www.schneider-electric.us/en/download/
  2. DO NOT TYPE ANYTHING  in either search box.
  3. To the right of Optional Filters, click "+".
  4. "Select Document Type Group"  - SKIP DO NOT SELECT ANYTHING.
  5. "Select Product Category" - choose Circuit breakers.
  6. "Select Product Sub-Category" - choose breaker type (such as Molded Case Circuit Breakers).
  7. "Select Product" - choose the breaker type (such as Powerpact P).
  8. Go back up to the top of the page, and click the large blue "Search" box (another page will open).
  9. On that page, at the left under "Document Type Group", beside the blue "More options", click "+".
  10. At the left, click "Technical Publications".
  11. At the left, beside "Document Type" click the "+".
  12. At the left, click "Tripping curves".
  13. Select the desired curves.
Was this helpful?
What can we do to improve the information ?