Technical FAQs

Ask a Question

Do the NSYEB power distribution blocks meet feeder circuit spacing requirements?

Issue:
Can the NSYEB blocks be used to feed service equipment? 

Product Line:
NSYEB Finger Safe Power Distribution Blocks

Environment:
North American Products

Cause:
Product Selection

Resolution:
Yes, most of the NSYEB blocks are listed to UL 1953.
With the NSYE Listed  enclosed blocks it is important to note that these are suitable for the Load Side of service equipment. They are  not certified for the Line Side of service equipment.
 

Was this helpful?
What can we do to improve the information ?