Technical FAQs

Ask a Question

What does CPH mean in my Wiser Air thermostat?

Question
What does CPH mean in my Wiser Air thermostat?
 
Answer
Issue:
Advanced settings in Wiser Air thermostat should only be adjusted with knowledge of setting changes.

Product Line:
Wiser Air residential thermostat

Environment:
Smart thermostat

Cause:
Advanced settings will alter the way the thermostat operates the HVAC system. Do not adjust CPH settings unless you understand CPH operations.

Resolution:
 
Compressor CPH
 
In normal operation, it represents the typical number of cycles that the equipment will turned on and off in one hour. The dead band on the Wiser Air is 3°F and it is not adjustable.
 





 
W, W2 Heating CPH

 
It represents the typical number of cycles that the equipment will turned on and off in one hour. The dead band on the Wiser Air is 3˚F and it is not adjustable.
 
Was this helpful?
What can we do to improve the information ?