Technical FAQs

Ask a Question

How do you change the Decel time on a ATV303 drive?

Issue:  
How do you change the Decel time on a ATV303 drive?
 
Product Line:
ATV303 drives
 
Environment:
All
 
Cause:
Parameter settings

Resolution:
From RDY press knob, then turn to CONF. Press knob, then turn to FULL. Press knob then turn to 500 (FUN). Press knob, then turn to 501 (Ramp). Press knob then turn to 501.1 (Decel). Press knob, make desired adjustments in seconds, press knob to confirm. Escape back to RDY
Was this helpful?
What can we do to improve the information ?