Technical FAQs

Ask a Question

Is there an extended I/O module for the ATV630?

Issue:
What is the part number for the I/O extension module for the ATV630 drive?
 
Product Line: 
ATV6xx Process drive
 
Environment: 
Is there an extended I/O module for the ATV630?
 
Cause:
N/A

 
Resolution:
The module with digital and analog I/O is VW3A3203. The module with Relay outputs is VW3A3204
 
Was this helpful?
What can we do to improve the information ?