Technical FAQs

Ask a Question

Are the S-Flex available in a Nema 12 enclosure?

Issue:
Are the S-Flex available  in a Nema 12 enclosure?

Product Line:
S-Flex

Environment:
Nema 12

Cause:
n/a

Resolution:
Yes, They are available in Nema 1, Nema 12, and Nema 3R.
Nema 12 and 3R units have a longer lead time because they are not stocked and must be built to order through product selector.

 
Was this helpful?
What can we do to improve the information ?