Technical FAQs

Ask a Question

Why does the motor rated current value for ATS22 in Somove not show correct value?

Issue:
Using ATS22 with SoMove: Does not show the accurate "Motor Rated Current." and changed the In setting and it reverts back to the original setting in SoMove.

Product Line:
ATS22

Environment:
SoMove

Cause:
Not showing the correct values on the SoMove printout

Resolution:
This is result of the Altistart DTM library being out of date.  Please download and update the catalog withing SOmove.  
The customer needs to update their DTM library to V12.0 minimum.
Was this helpful?
What can we do to improve the information ?