Technical FAQs

Ask a Question

S-Flex: What would cause motor wires to get hot?

Issue:
What would cause motor wires to get hot?

Product Line:
ATV212, S-Flex

Environment:
All

Cause:
Raceway and wires are getting very hot and motor is noisy.

Resolution:
Ensure proper wire gauging for motor voltage and amperage.

Check switching frequency parameter F300
-Lower for electrical
-Raise for audible noise

Check and make sure motor plate matches drive parameters.

 
Was this helpful?
What can we do to improve the information ?