Technical FAQs

Ask a Question

What is a Type 3 Surge Protection Device?

Product Line: 
Surge Protective Devices (SPD's)

Resolution:
Point of use SPD's, installed at a minimum conductor length of 10 meters (30 feet) from the electrical service panel. Surge protection plug in strips and receptacles are classified as Type 3.
 
Was this helpful?
What can we do to improve the information ?