Technical FAQs

Ask a Question

Getting Error 26 when installing engineering client for PME 7.2.2.

Issue
Following error message:

Cannot create nom register instance.

A network-related or instance-specific error occurred while establishing a connection to SQL Server. The server was not found or was not accessible. Verify that the instance name is correct and that SQL Server is configured to allow remote connections. [provider: SQL Network interfaces, error 26 - Error Locating Server/Instance Specified).


Product Line
SQL Server

Environment
Remote Access

Cause
SQL Server Browser is not running.

Resolution
Enable the SQL Server Browser service inside of "Services" on the server platform by starting it.
       To Locate the services screen
  1. Click the Start Menu and type “service.msc”. Or Click Run and type  “service.msc”.
  2. Locate the service SQL server browser.
  3. Double click the service.
  4. Change startup type to Automatic if not already set.



 
Was this helpful?
What can we do to improve the information ?