Technical FAQs

Ask a Question

Magelis HMISTU boots to the message Runtime Unsupported : The hardware platform does not match the target type defined in the application. Is there a way to recover from this?

Issue:
HMISTU boots to the message Runtime Unsupported : The hardware platform does not match the target type defined in the application.  Is there a way to recover from this?

Product Line:
HMISTU655/855, HMIS5T

Resolution:
The HMISTU targets does not have a way to recover the Runtime.  It is recommend that the unit be sent in for repair or get a replacement HMIS5T.
Was this helpful?
What can we do to improve the information ?