Technical FAQs

Ask a Question

Is the actuator part number: MA-230-0-2-1 still available?

Issue :
Is the actuator part number MA-230-0-2-1 still available?


Product Line
Valve and Actuators

Environment: 
Maintnance 

Cause: 
Replacement/Cross.

Resolution: 
The MA-230-0-2-1 was a Fire & Smoke actuator, which is no longer available . The Actuator was sold as an OEM Damper actuator ONLY and were only sold to Damper manufactures.
To get a replacement , you will need to find out who The Damper manufacturer is and call them for a replacement. 
 
Was this helpful?
What can we do to improve the information ?