Technical FAQs

Ask a Question

Video: How to upgrade the Link 150 firmware?

Issue:
How to upgrade the Link 150 firmware?

Product Line:
Link 150 (EGX150)

Environment:
Firmware upgrade

Resolution:


 
  1. Download the latest Link 150 firmware zip file attached below. 
    It can also be downloaded from this link
  2. Unzip the folder and store it in your local PC.
  3. Open the unzipped folder.
  4. Right-click the FirmwareUpgrade.bat, and then click Edit.
  5. Set the IP address, FTP user name, and password of the module being upgraded in the FirmwareUpgrade.bat file.
  6. Save and exit the FirmwareUpgrade.bat.
  7. Double-click the FirwareUpgrade.bat file, this starts the upgrade process. 
  8. Wait until the FirwareUpgrade.bat closes itself.
  9. After successful firmware upgrades, the Link 150 will take 40 seconds to restart. 
Note:
  • Default IP address = 169.254.YY.ZZ where YY and ZZ are the last two bits of the Link 150 MAC address. 
  • Default FTP user name = Administrator
  • Default FTP password = Gateway
Was this helpful?
What can we do to improve the information ?