Browse FAQs

How to determine the actual model number of a PM5000 meter?

Published date: 20 September 2019

Issue:

 The PM5000 Series meter's front display label may be misleading from the actual model number. The display will show just the family of the series as PM5x00.  

 Product Line:

PM5100, PM5110, PM5310, PM5320, PM5330, PM5340, PM5560, PM5563

Environment:

 Front display

 Cause:

 The meter's front display is labeled just with the corresponding family and not the model number.  

Resolution: 

Please refer to the serial number label on the side of the meter to see the meter's model number. If the meter is powered up you can use the front display to navigate to the information window:
Maint --> Diag ---> Info




Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.