Technical FAQs

Ask a Question

How Can I Change the Device ID in the ATV61 Bacnet card?

Issue:
How Can I Change the Device ID in the ATV61 Bacnet card?

Product Line:
All ATV61 drives

Environment:
Bacnet card

Cause:
Cannot change the Device ID

Resolution:
On ATV61 Bacnet card before V1.1IE09, apply the workarround in attachement

But since ATV61 Bacnet card V1.1IE09 we make an evolution, now the device name will be unique on the network (even if it can not be change directly by the user)
The BACnet address is added in the "ObjectName" property of the DeviceObject.
This will allow the user to distinguish many ATV61 on the same network.
The "ObjectName" property is now formatted as "ATV 61_xxx", where xxx is the BACnet drive address (from 0 to 127).

The ATV61 cards produced after the 29th of October 2014 have this V1.1IE09.
Was this helpful?
What can we do to improve the information ?