Technical FAQs

Ask a Question

What is F1 button assigned to "code" function?

Issue:
What is F1 button assigned to "code"  function?

Product Line:
ATV71  ATV61

Environment:
All

Cause:
NA

Resolution:
Code F1 Displays the code of the selected parameter, i.e., the code corresponding to the 7-segment display.
Was this helpful?
What can we do to improve the information ?