Technical FAQs

Ask a Question

DUPLICATE: FA263477 What are the part numbers for Thyristor and Diode modules for the 900 HP ATV61HC63N4 drive?

Issue:
What are the part numbers for Thyristor and Diode modules for the 900 HP ATV61HC63N4 drive?

Product Line:
Altivar ATV61

Environment:
All

Cause:
Input is shorted so they need replacement Thyristor and diode parts.

Resolution:
Thyristor Rectifier module is part number VZ3TM1600M1671 qty 6 are needed for one drive.
and
Diode module  is part number VZ3DM1600M1671 qty 6 are needed for one drive.

Was this helpful?
What can we do to improve the information ?