Browse FAQs

Can I add an expansion rack to an existing Quantum RIO drop using the CCOTF option?

Published date: 30 September 2019

No. It is not possible to add an expansion rack (140XBPxxx xx) to an existing Quantum RIO drop using CCOTF.


Legacy KB System (APS) Data: RESL209870 V1.0, Originally authored by DaSo on 12/04/2012, Last Edited by DaSo on 12/04/2012
Related ranges: Unity Pro - SoCollaborative software

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.