Technical FAQs

Ask a Question

What is the wire size for an NF250FTL feed through lug kit for an NF panel?

Issue:
For the NF250FTL lug kit, what is the wire size?

Product line:
NF panelboard accessories.

Environment:
NF panelboards used in the North American markets.

Cause:
Wire sizes needed for the terminals on the NF250FTL feed through lug kit.

Resolution:
The 250A feed through lug kit will accept (1) #6-350kcmil AL or CU wire.

See instruction bulletin, 80043-757-02


 
Was this helpful?
What can we do to improve the information ?