Technical FAQs

Ask a Question

Rejected Duplicate FA231381:Can I get a conduit kit for an ATV61/71 frame size 14 and 15?

Issue:
Rejected Duplicate FA231381:Can I get a conduit kit for an ATV61/71 frame size 14 and 15?

Product Line:
ATV61/71 Drives

Environment:
All serial numbers for ATV61/71 Drives

Cause:
N/A

Resolution:
No, the conduit kits for the ATV61/71 only go up to frame sizes 13

Was this helpful?
What can we do to improve the information ?