Technical FAQs

Ask a Question

Is there a Magelis HMIGTO 15" touch screen available?

There are no 15" scren available on the Magelis HMIGTO series.  The largest one is the HMIGTO6330 which is a 12".
The HMIGTU offers a 15" disolay. The HMIG3U with a HMIDT732 15" display.  This unit requires Vijeo Designer V6.2 SP2 or higher.
 
Was this helpful?
What can we do to improve the information ?