Technical FAQs

Ask a Question

Which cable do I use to connect an Magelis HMISTO501 to a Zelio Smart relay?

The communication cable is SR2CBL09.

The Magelis STO 501 terminal is dedicated exclusively to communication with Zelio
Logic SR2/SR3 range controllers.

This SR2CBL09 cable consist of two parts
1-SR2CBL08 cable
2) 4-wire cable screwed to the 9-pin connector which connects to the HMISTO501.
Was this helpful?
What can we do to improve the information ?