Technical FAQs

Ask a Question

REJECT - What are the fan kit part numbers for the ATV21HD30M3X, ATV212HD30M3X, ATV21HD55N4, ATV212HD55N4, ATV21HD75N4 and ATV212HD75N4?

Issue:
What are the fan kit part numbers for the ATV21HD30M3X, ATV212HD30M3X, ATV21HD55N4, ATV212HD55N4, ATV21HD75N4 and  ATV212HD75N4?

Product Line:
ATV212
Environment:
All serial numbers for ATV212, ATV21

Cause:
N/A
Resolution:
The part number for the fan kit is a VZ3V1208.
Was this helpful?
What can we do to improve the information ?