Technical FAQs

Ask a Question

Are all of the 9035, 9036, 9037 and 9038 float switches obsolete?

Issue:
Checking if all of the 9035, 9036, 9037 and 9038 float switches are obsolete.

Product Line:
9035, 9036, 9037 and 9038 Float Switches

Environment:
Pressure, Vacuum and Float Switches

Resolution:
No, After February 15th 2005 there are some 9035, 9036, 9037 and 9038 products that will be obsolete with no replacement. To check availability run the requested part number thru Q2C to see if it is still available.
 
Was this helpful?
What can we do to improve the information ?