Technical FAQs

Ask a Question

Does the ATV312.....M3 drive have an built in EMC Filter?

Issue:
The EMC filter is not installed on the ATV312H….M3 versions VFD

Product line: 
ATV312

Environment: 
All ATV312H…M3   

Cause:
The EMC is missing from the installation

Resolution:
The mains reason on M3 version that there is no EMC filter is for leakage current .   When you integrate emc filter you improve the leakage current.  If the M3 was with integrated EMC filter you will have a too much leakage current.   So the choice was to suppress it.

Was this helpful?
What can we do to improve the information ?