Technical FAQs

Ask a Question

Low resistance or short circuit measured on output of XW inverter with no connection


I'm measuring low resistance / short circuit on the output of my XW inverter with no load wires connected. Is my inverter defective?


XW Hybrid Inverter Charger


Not necessarily. Low DC resistance is normal on the output of the XW inverter


The output transformer on the XW Inverter will appear to an ohm-meter as a low resistance or short circuit.
Was this helpful?
What can we do to improve the information ?