Technical FAQs

Ask a Question

Can I use Vijeo Designer V6.2 Webgate on a Microsoft Surface tablet running Internet Explorer?

No, The IE on the Microsoft Surface can't run Webgate because the Surface does not support ActiveX on which Webgate is based.
Was this helpful?
What can we do to improve the information ?