Technical FAQs

Ask a Question

Downloading firmware to a CM2000 Using DLF-101

Product Line
CM2000
DLF-101

Environment
Firmware Upgrade

Resolution
Please see attached document.

It is suggested that DLF-3000 is used for CM2000s firmware upgrades, if possible. Please see FA237920 for DLF-3000.

Was this helpful?
What can we do to improve the information ?