Technical FAQs

Ask a Question

Setting The Master Password on CM2000 Series Meters

Product Line
CM2000

Environment
Password

Resolution
The CM2000's master password should not be set to 9999. If 9999 is used, the Circuit Monitor will go into the Protected Mode which will only allow the configuration to be viewed and not changed.

Was this helpful?
What can we do to improve the information ?