Technical FAQs

Ask a Question

How to Connect to a MB+ network with PW32 on a remote PC using a MBX Gateway?

Connecting Using the MBX Gateway Driver

Facts and Changes

MBX Driver Suite v6.0

Causes and Fixes

Note: For information on how to setup the MBX Gateway Client and Server see the resolution entitled "How to connect remotely to a MB+ network via TCP/IP using the MBX Gateway driver".
To Connect to a MB+ Network with PW32 from a remote PC via the MBX Gateway you must chose the Adapter/Device number of the MBX Gateway Client in the Communication Setup.
First in the Project tree double click on Communications.



Under the Modbus Plus tab type in the Adapter number of the MBX Gateway Client and the MB+ address of the PLC you wish to connect to. Hit OK and go Online to the PLC.


Was this helpful?
What can we do to improve the information ?