Technical FAQs

Ask a Question

What is the pinout of the integrated CANopen port on the M340 PLC's BMXP342010/2030?

The pinout of the integrated CANopen port on the M340 PLC's BMXP342010/2030 is:


Was this helpful?
What can we do to improve the information ?