What are the part numbers for the M340 Terminal block and cables with flying leads?
The part numbers for the M340 Terminal block & cables with flying leads are:
BMXFTWx01 1 FTB terminal block preformed with one 20 wire cable with color coded flying leads.
BMXFCWx01 1 FCN connector preformed with one 20 wire cable with color coded flying leads.
BMXFCWx03 1 FCN connector preformed with two 20 wire cable with color coded flying leads.
where x is 3, 5, or 10 for 3 meter, 5 meters, or 10 meters.