Technical FAQs

Ask a Question

Can the Modbus port on the 170ADM54080 IO Base be used for XMIT or XXMIT functions?

No. This port is designed for use with motion control centers and has limited functionality. Control of the Modbus messaging is done via register manipulation with a limited set of Modbus commands. Please see 870USE00200 for information on this module. Neither Xmit nor XXmit can be directed at this port.

Was this helpful?
What can we do to improve the information ?