Technical FAQs

Ask a Question

*******Rejected. Duplicate case**************Is it possible connect a computer to one of several ATV's on a Modbus Network and monitor the drive with Power Suite ? What hardware is neccessery ?

Goals and Symptoms

Is it possible connect a computer to one of several ATV's on a Modbus Network and monitor the drive with Power Suite ? What hardware is neccessery ?

Facts and Changes

atv58 and Modbus communication monitored with Power Suite

Causes and Fixes

No, problem. You just need to use PowerSuite v1.5, the connector kit VW3A8106 and some taps ( ie TSXSCA62 or another ) but it's necessary to use another RS232/RS485 converter because the one's provided need the 10v supply from the inverter. I propose you to use the XGSZ24.


Legacy KB System (APS) Data: RESL158731 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?