Technical FAQs

Ask a Question

Can I mix voltage and current on the analog input base 170AAI03000?

Yes, the 170AAI03000 input base can accept both voltage and current analog input signals.
The wiring diagram shows the proper connections for each type of input.


If configuring with Unity Pro - double click on the module graphic and select Channel 0 where all 8 channel ranges are selected.
 

Was this helpful?
What can we do to improve the information ?