Technical FAQs

Ask a Question

REJECT - What is the conduit kit used for with a ATV212 drives?

Issue:
What is the conduit kit used for with a ATV212 drives?

Product Line:
ATV212

Environment:
All

Cause:
Need to make the drive Nema 1 rated

Resolution:
The conduit kit encloses the drive at the bottom and covers power wiring. The conduit kit provides Nema 1 rating (finger safe) to the drive.

Was this helpful?
What can we do to improve the information ?