Technical FAQs

Ask a Question

What are the dimensions for the J250DS, J250DSVW, J250SS and J250SSVW circuit breaker enclosures?

Issue:
Dimensions

Product Line:
Circuit Breaker Enclosure

Cause:
Dimensions

Resolution:
These enclosures are 32.26" H x 9.72" W x 5.61" D.

Click this link to access the Approval Drawing #3363S:
https://www.schneider-electric.us/en/download/document/3363S/
Was this helpful?
What can we do to improve the information ?