Technical FAQs

Ask a Question

What is the replacement for an HCN1436-4 I Line panelboard interior?

Issue:
What is the replacement for an HCN1436-4  I Line panelboard interior?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Maintenance.

Resolution:
Use a HCN14524. It has the same amount of branch mounting space and will fit in the old 36`` box. However, the original trim will not fit and there is no replacement trim available.


 
Was this helpful?
What can we do to improve the information ?