Technical FAQs

Ask a Question

What is the definition of IP55 ?

Issue:
What is the definition of IP55 ?

Product Line:
Altivar ATV630 ATV930

Environment:
All serial numbers

Cause:
Customer wanted to know what is IP 55 for IP degree of protection of ATV630? 

Resolution:
The first ``5`` is for Dust protection and the second  ``5`` is for protection against water jets in all directions.


 
Was this helpful?
What can we do to improve the information ?