Lexium® 15 Servo Drives and Motors

Servo drives with power range from 0.9 to 42.5 kW and voltage range from 200 to 480 V. BDH servo motors with nominal torque of 0.18 to 53 Nm (1.6 to 469 lb-in) and nominal speed of 1000 to 8000 rpm. Control Signals: Input/Output. Bus and Networks: CANopen, Profibus DP, Modbus Plus, FIPIO, Sercos, and Modbus TCP. Motion Bus: CANopen Motionbus.