Automation Components

Categories

Advantys™ STB Distributed I/O
OEM Solutions
Phaseo™ Power Supplies, Type ABL7
The ABL7 selection offers a comprehensive range from 0.3 A to 40 A.
Relays, Zelio® Logic
Zelio® Logic relays are more than typical relays. They accept inputs, have relay outputs like a programmable controller, and are designed for use in small automated systems. They areused in both industrial and commercial applications.
Twido™ Controllers
The Twido™ nano PLC is a hard-working ultra-compact controller designed especially for small control systems.